We Cut, Pull, and Deliver What You Need

Wire and Cable Services


Managing larger projects can get complicated. If you can make things easier, why wouldn't you? Elliott Electric Supply can drop off a truck loaded with cut and paralleled reels with pulling heads on A-Frames, ready for pulling. When you're finished or need a resupply, simply let us know and we'll meet you at your jobsite.

Elliott Electric Supply loads jobsite trailers with your inventory supplies

Elliott Electric Supply can customize wires, cables, and reels to your specifications, ensuring they fit the exact requirements of your project's needs, through every job phase. Our services can include wire cutting, wire paralleling, pulling heads installation, A-Frame Reel Rentals, and truck/trailer rentals to simplify your installation process. These services and more can be customized to fulfill your needs.

Our wire and cable services are vital to managing your projects through all job phases. We save you time, reduce waste, and ensure that materials are ready to use upon delivery. We help you meet your project deadlines by providing tailored solutions that eliminate the need for on-site adjustments.

Wire and Cable Service Features

Why Choose Elliott Electric Supply Wire Services?


Wire and Cable Cutting
Wire & Cable Cutting

Our dedicated wire cutting specialists can cut your wires and colored feeder cables to any length you need to fit the exact requirements of your project. We help you save time, reduce waste, and ensure materials are ready to use upon delivery.

Parallel Wire Reels
Wire & Cable Paralleling

Reduce the need for separate reels and reel jacks by using our wire and cable paralleling service. EES can bundle a custom configuration of multiple wires or cables onto a single reel (wooden spool or SIMpull™) to be pulled simultaneously. Paralleling cable not only speeds up the job, but also improves organization and efficiency.

Cable Pulling Heads
Wire & Cable Pulling Heads Installation

Our trained employees can pre-installed pulling heads on a cable reel. This eliminates the hassle of manually installing them later on and gives you peace-of-mind knowing our pulling heads are performing properly.

SIMpull™ Reel Rentals
SIMpull™ Reel Rentals

We rent SIMpull™ Reels which eliminates the need for reel jacks and axles because the outer flanges rotate independently of the inner reel. The outer flanges also rotate independently of each other making it easier to move the reel in tight spaces without a whole crew. The SIMpull™ Reel is narrow enough to fit through 36" doors on the job site, allowing you to place the reel right next to your feed conduit/point, reducing labor costs and time. SIMpull™ Reels also eliminate the need for pallet jacks.

Wire Stacking
Wire Stacking

When you have limited space, but require specific wiring for each job phase, we can stack each phase of parallel wires or feeder cable in the order you need them on a single reel with labeled shrink wrap between the layers for each phase. Although we can load up to 6,000 lbs on a single SIMpull Stack™ Reel, the reel is significantly easier and safer to move, because the outer flanges rotate independently, and rotate separately from the inner reel. We also handle wooden spool stacked reels.

Loaded Wire Pulling Truck or Trailer Rentals
A-Frame or Loaded Truck/Trailer Rentals

Save money on expensive equipment by using our A-Frame Reel Rental services. We will load an A-Frame with whatever reels you need for pick up. If you don't have the means (or don't want) to lug reels to your jobsite, you can rent a loaded trailer or truck for a few hours from Elliott Electric Supply. We can deliver a fully stocked wire pulling truck or trailer to your jobsite so you can pull wire right from the trailer, expediting your pulls.

Ready to Experience the Convenience of Our Wire Services?

Let's Get Started

Have Custom Wire or Cable Service Needs?


You're in good hands with Elliott Electric Supply. We specialize in customer service! Contact your customer service representative to start a conversation about the services you need.

Want to Save Even More Time and Money?

Our Wire Services vs Basic Installation


SIM<em>pull</em>™  Reels save money and time.
Save Time and Money with Simpull Reel
With Elliott Electric Supply, you can reduce the time of a wire pulling installation by up to 90%!* Saving Approximately 24 man-hours at $75/hour means a $1800 savings over a traditional wire pull installation!

Unwinding wire from a stationary reel can be a struggle and when not done properly, can cause larger and more costly problems later on and even lead to an unsafe work environment. Elliott Electric Supply offers SIMpull™ Reel rentals so you can unroll your wire with ease. The SIMpull™ Reel has independently rotating outer flanges and separately rotating inner reel, which eliminates the need for reel jacks and pallet jacks.

*Time-saving comparison data sourced from Southwire.com

Rent a SIMpull™ System from Elliott Electric Supply

Typically requires 3 people

Step 1 (1 man-hour): The reel of SIMpull™ THHN® cable with 5 parallel color conductors arrives at the job site and a team of three unloads the SIMpull™ Reel, transports it to the pull site, and, if required, levels the reel on jacks.

Step 2 (0.5 man-hours): Ropes and rags are pulled through the conduit.

Step 3 (0.05 man-hours): SIMpull™ Head® pulling grips get attached to pull ropes.

Step 4 (0.1 man-hours): Set up Maxis® cable puller.

Step 5 (1 man-hour): Start pulling cable (average pull speed is 12 feet per minute).

Total Time: 2.65 Man-Hours

Choose Basic Cable Pulling Installation

Typically requires 6 people

Step 1 (7 man-hours): 4 x 250 black conductors with ground wire arrive at the job site and a team of six has to transport the reels to the pull site and level them on jacks.

Step 2 (1 man-hour): Lube buckets and rags are delivered to the pull site.

Step 3 (0.05 man-hours): Phase tape is installed and circuits are inspected.

Step 4 (1 man-hour): Ropes and rags are pulled through the conduit.

Step 5 (5 man-hours): Set up the conductor head and attach it to pull ropes.

Step 6 (3 man-hours): Prepare the cable puller.

Step 7 (3 man-hours): Prepare lube to apply to the cable head and pull boxes.

Step 8 (4 man-hours): Begin pulling cable and applying lube to the two locations (pulling speed average 6 feet per minute).

Step 9 (1.5 man-hours): Clean lube off the conductors and enclosures.

Total Time: 25.55 Man-Hours

Save Time and Money with SIMpull Reel

How Much Time Will You Save?


25.55 MH with Basic Installation 2.65 MH with SIMpull™ Reel = 22.9 Man-Hours Saved

Learn How to Get Started Today
 

Explore Related Services for Your Projects


Explore More Elliott Electric Supply Services