Electric Motor Supplies - Components and Accessories
Electric Motor Components:
Electric Motor Accessories:
Electric motors convert electricity into mechanical energy and are used to power several kinds of devices, including running fans, power tools, home appliances, industrial equipment,
and more. They are powered by either direct current (DC) sources, such as batteries, or by alternating current (AC) sources, such as electrical generators. There are many
electric motor components, including power supplies, relays, contactors, terminal boxes, signaling devices like a bell, and more.
These motor supplies must meet certain standards and requirements per the International Electrotechnical Commission (IEC) and the National Electrical Manufacturers
Association (NEMA). Elliott Electric Supply offers a variety of electric motors that meet national and international standards as well accessories and add-on's for
electric motors.
Overload Relay
An overload protection relay safeguards an electric motor from overload or overcurrent damage. A overload relay protects a motor from overheating by halting the current flow with
restart delay options.
Shop Overload Relays
Timing Relay
A timing relay has a function that will delay current-flow once switched on. There are multiple types of timing relay. Elliott Electric Supply offers on/off delay, one shot, interval, and
recycle relay types.
Shop Timing Relays
Alternating Relay
An alternating relay, in contrast to a latching relay, requires a control switch and continuous power. An alternating relay is used to equalize run times or to run multiple loads
at the same time.
Shop Alternating Relays
↑ To Top
Electric Motor Terminal Blocks - Single Feed, Dual Level, Power Distribution, Grounding, etc.
Terminal Strip
A terminal strip is a device that connects wires to a panel or junction box.
Shop Terminal Strips
Fuse Holder
A fuse holder terminal block connects multiple fuses with multiple devices.
Shop Fuse Holders
Power Distribution Block
A power distribution terminal block, or power distribution box, is used to 'terminate' cables and wires.
Shop Power Distribution Blocks
Ground Clamp (Ground Circuit Terminal Block)
A ground circuit terminal block, or ground clamp, is used to ground electrical circuits.
Shop Ground Clamps
Disconnect Terminal Block
A disconnect terminal block, or switch block, is used to safely disconnect a circuit on a terminal without removing wiring.
Shop Disconnect Terminal Blocks
↑ To Top
Industrial Motor Controls - PLC & HMI Interface, Controller Hardware
↑ To Top
Motor Accessories - Rails, Enclosures, Signals
Electric motors can be paired with additional equipment and accessories. Below are some common add-on parts for use with electric motors.
↑ To Top
See Our Other Guides for Motors:
Learn More About Our Other Products: