Add More Items
View All Quick Selects
Step 1. Determine cavity ratios.
Cavity Ratio = (2.5 x height of cavity x cavity perimeter) / area of cavity base
Step 2. Determine effective cavity reflectances
Use the Effective Cavity Reflectance Chart below.
Step 3. Select coefficient of utilization
Use the manufacturer's tables with effective cavity reflections from Step 2 for specific fixture type.
Step 4. Find the Number of Fixtures Needed
Use formula below to determine appropriate number of fixtures.
Number of Fixtures = (room area in square feet x desired foot candles) / (lumens per fixture x coefficient of utilization)
Find recommended foot candles for indoor and outdoor locations.
Note: This method is used for estimating purposes only and other factors may contribute to resulting illuminance level. Refer to the IESNA Lighting Handbook for further details.
Shop Pendant Light Fixtures
Shop Downlight Fixtures
Shop Track Lights
Shop High Bay Fixtures
Shop Troffer Light Fixtures
Shop Light Fixtures and Parts
Shop Fluorescent Lamps
Shop LED Lamps
Shop Incandescent Lamps
Warning: When using this information to perform electrical work, call a licensed electrician and consult the NEC® for safety. All licensed electricians have passed examinations covering the National Electric Code®, know state and local building codes, and may carry insurance to cover damages.