Maximum Current Adjustment Factors for More Than 3 Current Carrying Wire Conductors


To calculate the maximum current in an insulated wire when there are more than 3 current carrying wire conductors in the same raceway or cable, first, find the maximum allowable current for a raceway or cable with less than 3 current carrying wire conductors, then multiply that maximum current by the percentage number from the Adjustment Factors for More Than 3 Current Carrying Conductors Chart below and divide by 100.

Maximum Current Adjustment Factors for More Than 3 Current‑Carrying Conductors in a Raceway or Cable

Number of Conductors in a Raceway Percent of Total Value
4 – 6 80
7 – 9 70
10 – 20 50
21 – 30 45
31 – 40 40
41 or Above 35

Table 310.15(C)(1), 2020 NEC®


Shop Related Products

Building Wire

compressed stranded copper wire

Shop All Building Wire

Meters and Testers

Cable tester electric meter kit

Shop Meters & Testers

WARNING: For safety, call a licensed electrician and consult the NEC®. All licensed electricians have passed examinations covering the National Electric Code®, know state and local building codes, and may carry insurance to cover damages.