Add More Items
View All Quick Selects
A conduit bender is a hand-held tool that allows users to easily reshape EMT conduit. Conduit is inserted into the bender's head and, following the specialized guides, the user will step on the foot pedal or use their hands to bend the metal pipe at whatever angle they need. Additionally, the bender's long handle can be used to straighten conduit.
Shop EMT Conduit Benders
A = Rim notch or teardrop -- Locates the center of a 3-point saddle bend.
B = Arrow -- Used to line up the offset and outer marks for saddle bend.
C = Star -- Indicates back of 90° bend, for back-to-back bends.
D = Marks -- The degree marks indicating the angle of the pipe bent.
How to make a 90° bend with EMT, also called a stub up, or an accurate stub.
Words to know
1. Measure the desired stub height. For this example, the stub height is 11" on a ½" pipe (Figure 1).
2. Subtract take-up from the desired stub height to calculate the starting point for the bend from the end of the pipe. To make an 11", 90 degree bend with 1/2" tube, allow 5" for take-up. Mark bend starting point on conduit (a distance of 6" from the end of the pipe for our example).
NOTE: With a ¾" pipe, allow 6". With a 1" pipe, allow 8".
3. Place the bender on the ground with the handle in the air.
Figure 1
4. Slide the pipe into the bender and align the right side of the mark with the bender's arrow (B), as shown in Figure 2.
Figure 2
5. Step onto the back end of the pipe.
6. Place the other foot on the back of the foot pedal to apply pressure.
7. Pull back on the handle until the end of the pipe rises vertically as shown in (Figure 3). In a 90° bend, the pipe will be shaped like an "L".
Figure 3
A box offset is a small Z-shaped bend and is commonly used on conduit connecting to an outlet box.
An offset is a bending technique that turns a straight conduit into a Z-shape, which allows it to avoid obstacles and change elevation.
A back-to-back bend uses two stub bends in the same direction to make a U-shape.
C = Center point for finished saddle bend
X = Double the length of the diameter of C
Y = Double the length of the diameter of C
Example: If the diameter of C is 10", then the length from C to X should be 20" and the length from C to Y should be 20". The total length between X and Y will be 40".
1. Calculate and mark where the pipe will be bent.
2. Slide the tube into the bender until the C mark on the tube is centered on the A notch on the bender.
3. Pushing on the pipe close to the bender, bend the Y side of the pipe down to a 45° angle.
NOTE: A 45° bend is reached when the bender handle is at a right angle to the tube.
4. Reverse the tube in the bender and align the X mark on the tube with the bender arrow at B.
5. Make a backward or return bend of 22 ½°.
6. Repeat step 4 and step 5 on the Y mark.
6. Proper alignment and bending of the C, X, and Y guidelines will result in the remaining pipe returning to a straight line.
Shop EMT Conduit
Shop EMT Connectors
Shop EMT Straps and Clamps
Shop EMT Couplings
Warning: When using this information to perform electrical work, call a licensed electrician and consult the NEC® for safety. All licensed electricians have passed examinations covering the National Electric Code®, know state and local building codes, and may carry insurance to cover damages.