Types of Data Network Cable (STP - UTP - Coax - Fiber Optic Cables)


When choosing a network cable, it's important to assess key factors such as the networking environment (interference levels), required bandwidth, distance, security considerations, and budget constraints. Each cable type has its advantages and is tailored for different use cases, so understanding these technical distinctions will guide your decision-making process effectively.

UTP Ethernet Cable: Unshielded Twisted Pair

What is UTP Cable?

A UTP network cable is a type of data cable used for transmitting data in computer networks. A UTP cable consists of pairs of insulated copper wires twisted together without shielding on the twisted pair or outer shielding on the cable.

Advantages of UTP Cable:

  • UTP cable is a cost-effective cable solution.
  • Without a shield, UTP cable is fairly flexible and easy to install.
  • 22 gauge UTP cable and 24 gauge UTP cable are commonly used and readily available.

Disadvantages of UTP Cable:

  • UTP cable is vulnerable to EMI and RFI interference, which can cause transmission errors and performance issues.
  • UTP Cable has limited bandwidth, which translates into slower transmissions.
  • Without a shield, UTP cable is somewhat vulnerable to security breaches.

STP Ethernet Cable: Shielded Twisted Pair

What is STP Cable?

An STP network cable is an Ethernet cable that has shielding around the twisted pairs of copper wires or outer shielding under the cable jacket to reduce electromagnetic interference (EMI) and radio frequency interference (RFI) in environments with higher interference levels.

Advantages of STP Cable:

  • Due to reduced noise, STP cables offer better signal integrity over distances up to 100 meters.
  • STP shielding makes the cable more resistant to physical damage.
  • Because of its shielding, STP cable is better protected against EMI, crosstalk, and RFI interference.
  • The shielding in STP cable helps prevent data leakage and unauthorized access.

Disadvantages of STP Cable:

  • STP cable is generally more expensive than UTP cables due to the additional shielding.
  • The shielding inside STP cable makes it less flexible and slightly more difficult to bend.
  • Terminating STP cables requires professional expertise and specialized tools.

Coax Cable

What is Coax Cable?

A coaxial (coax) cable is used to transmit high-frequency electrical signals with low loss and minimal interference, making it suitable for applications such as cable television, internet (cable internet), and certain types of networking.

Advantages of Coax Cable:

  • Coax cable can support longer transmission distances compared to UTP and STP cables.
  • Because of their enhanced shielding, coaxial cables have a better resistance to EMI and RFI interference.
  • Coax cable can support higher bandwidth capacities for applications requiring high data transfer rates like CATV.
  • Coax may be a cheaper option than fiber optic cable.

Disadvantages of Coax Cable:

  • Coax is slower and less reliable than fiber optic cables.
  • Compared to UTP and STP cable, coax cable is thicker and less flexible, which can make their installation more challenging.
  • Over long distances, coaxial cable may require the use of signal boosters due to signal loss.

Fiber Optic Cable

What is Fiber Optic Cable?

A fiber optic cable transmits data using pulses of light over long distances with minimal loss, offering high bandwidth and immunity to electromagnetic interference. Fiber Optic Cable is ideal for high-speed telecommunications and networking applications.

Advantages of Fiber Optic Cable:

  • Fiber optic cables experience minimal signal loss over long distances due to low attenuation.
  • The high bandwidth of fiber optic cable can support very high data rates in the gigabit range.
  • Fiber optic cables do not conduct electricity.
  • Fiber optic cables do not radiate electromagnetic signals, which enhances data security.
  • Fiber optic cables are ideal for high-speed data transmission over long distances.
  • Because fiber optic cables lack a metal conductor, fiber optic cables are lightweight and thin compared to other cables.

Disadvantages of Fiber Optic Cable:

  • Fiber optic cables are generally more expensive than copper cables.
  • Fiber optic cables are fragile and can be damaged by over-bending or crushing.
  • Light loss can occur at connectors and splices in fiber optic cables.

Shop Related Products

UTP Cat Cable

utp cat network cable

Shop UTP Cable

CAT Cable Crimper/Cutter

data cable crimper, stripper, and cutter

Shop Cable Cutter Tool

RJ45 Connector

RJ45 Connector Shop RJ45 Connectors

Cable Tester

Cable Tester Shop Cable Testers

Cable Tray

Cable tray Shop Cable Trays

Warning: When using this information to perform electrical work, call a licensed electrician and consult the NEC® for safety. All licensed electricians have passed examinations covering the National Electric Code®, know state and local building codes, and may carry insurance to cover damages.